cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-H743ZI2 NRND and use NUCLEO-H753ZI

senra
Associate

Hi ,

Does project files compiled and created in NUCLEO-H753ZI require any modification or recreation of project files when ported to STM32H743ZI.

3 REPLIES 3
STTwo-32
ST Employee

Hello @senra and welcome to the ST Community :smiling_face_with_smiling_eyes:.

The difference between both STM32H743ZI and STM32H753ZI is the Crypto part. So, if you have a project on the STM32H753ZI without a Crypto implementation, you can migrate it to the STM32H743ZI without a problem.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Is the NUCLEO-H743ZI2 (MB1364B, ST-LINK/V3) really NRND? I see the NUCLEO-H743ZI (MB1137, ST-LINK/V2-1) one is, and that's not surprising, but the ZI2 doesn't have it's own landing page  https://www.st.com/en/evaluation-tools/nucleo-h743zi.html

As I recall the STM32H753ZI is based on the ZI2 (MB1364B) board, so there's going to be a handful of different pins related to LEDs and QSPI, as I recall.  https://www.st.com/en/evaluation-tools/nucleo-h753zi.html

There's a USE_XYZ type define to select between the board designs at the NUCLEO.H level

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hello @Tesla DeLorean 

The NUCLEO-H743ZI2 is an NRND product:

STTwo32_0-1717171003631.png

The NUCLEO-H743ZI is an Obsolete product:

STTwo32_1-1717171058219.png

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.