2024-06-23 10:19 PM
NUCLEO-F412ZG Operating temperature Range?
I want to test my target control IC over a specific temperature range.
I would like to know the operating range of NUCLEO.
2024-06-23 11:08 PM
Hello @KMin .1
The NUCLEO-F412ZG is base on the STM32F412ZGT6 MCU. So, it has an Industrial temperature range of -40 to 85 °C. You can check this on the ordering information chapter of the DS11139.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-24 09:14 AM - edited 2024-06-24 09:39 AM
Becarefull:
You said "NUCLEO-F412ZG Operating temperature Range". So this includes all the components (parts/connectors etc ..) on the board not only the MCU.
The information given by @STTwo-32 is just for the MCU.
2024-06-24 09:27 AM
@SofLit wrote:The information given provided by @STTwo-32 is just for the MCU.
Indeed.
@KMin .1 you can download the BoM from the 'CAD Resources' tab on the 'Product Page':
https://www.st.com/en/evaluation-tools/nucleo-f412zg.html#cad-resources
2024-06-24 09:28 AM
@KMin .1 wrote:I want to test my target control IC over a specific temperature range.
What temperature range, specifically?