cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-C031C6 duplicate net name on Morpho connector

Karl Yamashita
Principal

 

I believe that the net name on CN7-4 should be PD3. 

Nucleo-C031_doubleNetname.jpg

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.
1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Karl Yamashita @Andrew Neil 

After checking with our HW team, I can confirm that both connectors CN7-3 and CN7-4 are mapped to the same pin of the MCU (PD2).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
STTwo-32
ST Employee

Hello @Karl Yamashita 

Thank you for this contribution. I'm checking internally and i will be back to you ASAP.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Fig 7 in UM2953 is the same:

AndrewNeil_1-1727801087393.png

 

PS:

PD3 is on CN10.1 both in schematic and in UM2953 Fig 7

 

STTwo-32
ST Employee

Hello @Karl Yamashita @Andrew Neil 

After checking with our HW team, I can confirm that both connectors CN7-3 and CN7-4 are mapped to the same pin of the MCU (PD2).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Karl Yamashita
Principal

As @Andrew Neil, PD3 is on CN10, which i missed.

Though it doesn't make sense to have PD3 by itself when it could have been grouped with the other 3 PDx pins. Unless there is a reason to have PD3 on CN10?

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.