Skip to main content
AQue
Associate II
September 26, 2024
Solved

Load external flash from command line

  • September 26, 2024
  • 2 replies
  • 1794 views

I have an STM32H7B31-EVAL board setup with TouchGFX.  I am able to compile and load a project using STM32CubeIDE.  I would like to be able to do the same from the command line.  I found this document that gives a very basic outline of the STM32_Programmer_CLI program.  I am able to load the MCU portion of the program this way, but I can't find any documentation on how to use it to load the external flash.  In CubeIDE, I have an external loader selected (MX25LM51245G_STM32H7B3I-EVAL-REVB.stldr).  I'm not sure how to use this setup from the command line.  Links to documentation or existing solutions would be appreciated. 

This topic has been closed for replies.
Best answer by Tesla DeLorean

Takes the form of the following to read the content out, --download variant to program, will  find an example

 

STM32_Programmer_CLI -c port=swd --vb 3 --log test_5m6.log --extload C:\STM32Cube\STM32CubeProgrammer_v2.10.0\bin\ExternalLoader\CLIVEONE-W25Q512_STM32L4XX-PB10-PA2-PE12-PB0-PE14-PE15.stldr --upload 0x90000000 0x559298 test_5m6.bin

See attached command line help screen

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
September 26, 2024

Takes the form of the following to read the content out, --download variant to program, will  find an example

 

STM32_Programmer_CLI -c port=swd --vb 3 --log test_5m6.log --extload C:\STM32Cube\STM32CubeProgrammer_v2.10.0\bin\ExternalLoader\CLIVEONE-W25Q512_STM32L4XX-PB10-PA2-PE12-PB0-PE14-PE15.stldr --upload 0x90000000 0x559298 test_5m6.bin

See attached command line help screen

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
AQue
AQueAuthor
Associate II
October 2, 2024

For my specific setup, I did the following: 

./STM32_Programmer_CLI -c port=SWD freq=8000 reset=HWrst \
--extload ./ExternalLoader/MX25LM51245G_STM32H7B3I-EVAL-REVB.stldr \
-w /path/to/file.hex

Note that the STM32_Programmer_CLI program needs to be run from the its directory (at least in Linux).  For example, I have the utility in /opt/stm32/bin.  Not being in this directory will result in error messages like "Unable to list supported devices". 

 

Thanks for the assistance.