2020-01-29 9:41 PM
I have given 3.3V to all VDD,VDDA,VBAT,VREF+ with capacitive filtering (100 nf & 1uf) as per datasheet. BOOT0 pin is connected to GND. SWDIO and SWCLK connected to debugger pins. Still it is giving same error.
when BOOT0=1, flashing is done but it gives debugging problem.In debugging mode, debugger does not display data of registers.
Please give me the solution for this error.
2020-01-29 9:45 PM
Make sure the ST-LINK/V2 Pin 1 or 2 are connected to VDD
Check signal level on NRST
Check voltages on VCAP pins
2020-01-29 9:52 PM
recommend voltages on vcap1 and vcap2 for stm32f401vbt6