2020-04-01 5:40 AM
For educational purpose, I want to make a STM32F103 board.
I'm going to design, make, and sell them.
To use ST's reference project also, the nucleo schematic can be the best reference.
If I make a STM32F103 board based on nucleo schematic (remove STLINK, addh LED and some other user in/out components),
is there any copy-right issue or other problem ?
2020-04-02 2:59 AM
There are zillions of F103 boards out there. Design and make is a good exercise, but selling them will take more than the bare will to do so, BluePill board start at a very low price!