2025-07-29 6:28 AM
Hello,
I'm working with the X-NUCLEO-WB05KN1 shield connected to a STM32 Nucleo board.
My goal is to build a simple demo:
Toggle an LED from a smartphone command
Send a notification to the smartphone when the User button is pressed.
I would like to use STM32 BLE Toolbox as the smartphone application.
Which firmware binary should I flash on the WB05 shield to ensure compatibility with STM32 BLE Toolbox?
From what I’ve read, the BLE_TransparentMode_UART_with_Updater.hex firmware from X-CUBE-WB5N V2.0.0 seems suitable — can you confirm this, and indicate the exact file to flash?
I can also flash :
- BLE_TransparentMode_UART_for_Updater.bin
- BLE_TransparentMode_UART_for_Updater_C_O.bin and BLE_TransparentMode_UART_with_Updater_C_O.hex
- DTM_UART_WITH_UPDATER.bin and DTM_UART_WITH_UPDATER.hex
- DTM_UART_WITH_UPDATER_CONTROLLER.bin and DTM_UART_WITH_UPDATER_CONTROLLER.hex
Thanks in advance for your support!
Best regards,
Sheul
Solved! Go to Solution.
2025-08-08 12:01 AM
Hello sheulisback,
your demo can be built on an SampleApp example, which creates the central/peripheral relationship between board and smartphone.
Speaking of firmware, both BLE_TransparentMode_UART_with_Updater.hex and BLE_TransparentMode_UART_with_Updater.hex are suitable for communication with ST BLE ToolBox.
2025-08-08 12:01 AM
Hello sheulisback,
your demo can be built on an SampleApp example, which creates the central/peripheral relationship between board and smartphone.
Speaking of firmware, both BLE_TransparentMode_UART_with_Updater.hex and BLE_TransparentMode_UART_with_Updater.hex are suitable for communication with ST BLE ToolBox.