2017-09-15 02:53 AM
I'm working with a Nucleo F411RE.
I've setted JP5 to E5V than I have power up the board from VIN pin.
My Chip and application works well, but the STLINK board still working without USB. I can see the Red Led (LD1) flashing.
If I measure power consumption on IDD connector I read 13mA, but If I read power consumption direcly from E5V I read 70mA.
Is possible to turn off the STLINK without cut it off from the board?
Really thank you.
#nucleo #stlinkv2(v2)2017-09-15 03:12 AM
Remove D3, SB12, R23 and SB13/14
D3 removes E5V from the ST Link.
SB12 remove the unpowered STlink from pulling NRST low.
R23 removes the connection from the target 3.3 Volt to the STlink ADC.
SB13/14 are other connections from the target to none 5 Volt tolerant pins.
I hope I didn not forget any other target <-> Stlink connection regarding none 5 Volt tolerant pins.
SB13/14 can remain, if the target keeps these line low.