2020-02-07 04:58 PM
Hi!
I did buy a Chinese clone "Blue Pill" that are supposed to work as a real STM32. When I looked at the chip, it was not a STM32 chip. It was a CS32F103C8T6 chip instead of STM32F103C8T6
Now I'm have connecting the ST-link from my Nucleo board to the Blue Pill, and the ST-link cannot recognize the Blue Pill board.
Vendor = 0x3B
Error in initializing ST-LINK device.
Reason: ST-LINK: Could not verify ST device! Abort connection.
Does that mean that it's NOT possible to program these Chinese clones with ST-Link and CubeMX, or is there a walk around?
I can see that lots of people have the same issue.
https://forum.atollic.com/viewtopic.php?t=1651
Link to the Blue Pill
2020-02-09 09:28 AM
You should better ask the chinese clone forum.