2022-10-11 06:50 AM
In other words, is the Zio a subset of the Morpho?
Solved! Go to Solution.
2022-10-11 07:42 AM
Welcome, @ARivero, to the community!
Your are currently talking about the NUCLEO-H723ZG, correct?
Yes, ZIO is a subset of the MORPHO connectors, also the 5V and VIN connections that do not belong to the STM32H723 are brought out on both connectors.
Does it answer your question?
Regards
/Peter
2022-10-11 07:42 AM
Welcome, @ARivero, to the community!
Your are currently talking about the NUCLEO-H723ZG, correct?
Yes, ZIO is a subset of the MORPHO connectors, also the 5V and VIN connections that do not belong to the STM32H723 are brought out on both connectors.
Does it answer your question?
Regards
/Peter
2022-10-11 09:36 AM
Hi Peter,
correct I'm using that Eval-Kit.
and, yes, that was the answer I was looking for. Is there any explicit written section in the documentation that states this?
Many thanks!
2022-10-11 11:29 AM
I am not aware of any explicit statement on this in the documentation. However, it is quite easy to check this by creating, sorting and comparing tables of pin assignments and functions.
Regards
/Peter
2022-10-11 10:15 PM
In fact, we did that way with the tables, I was wondering if there was something explicit about Zio and Morpho to avoid doing that task.
Thanks for confirm that.
Regards
2022-10-12 04:29 AM
OK. If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter