cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F405: exit low power STOP mode on external interrupt pin

lan1
Associate II

Hello,

I want to use the PB6 pin as an external interrupt input. When the PB6 pin is triggered, the program enters the low-power stop mode from the normal operation mode. When it is triggered again, the program enters the normal operation mode from the low-power stop mode. According to the above, the test found that after the program enters the low-power mode, it cannot return to the normal operation mode again.

 

Does anyone have experience in this area and can provide me with a solution?

1 ACCEPTED SOLUTION

Accepted Solutions

@QSHAO.1  @TDK   hello I configured PB6 as an external input interrupt. The configuration is as follows, and I am certain that this function is normal and effective.

EXTI_InitTypeDef EXTI_InitStructure;
  NVIC_InitTypeDef NVIC_InitStructure;


  RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);


  SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOB, EXTI_PinSource6);

  EXTI_InitStructure.EXTI_Line = EXTI_Line6;
  EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;
  EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling;
  EXTI_InitStructure.EXTI_LineCmd = ENABLE;
  EXTI_Init(&EXTI_InitStructure);

  NVIC_PriorityGroupConfig(NVIC_PriorityGroup_4);


  NVIC_InitStructure.NVIC_IRQChannel = EXTI9_5_IRQn;
  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x03;
  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x03;
  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
  NVIC_Init(&NVIC_InitStructure);

 And I placed the low-power mode in the time slice polling. Meanwhile, the PB6 pin is self-resetting and will only be triggered once at a time.

 PWR_EnterSTOPMode(PWR_Regulator_LowPower, PWR_STOPEntry_WFI);
    SystemInit();

View solution in original post

6 REPLIES 6
TDK
Super User

Don't enter low-power mode from within an interrupt. Set a flag and do it in the main thread.

Additionally, if this is a button, you will probably have to debounce it.

If you feel a post has answered your question, please click "Accept as Solution".
QSHAO.1
ST Employee

Some information about how to exist stop mode (refer to RM0090), hope it's helpful.

If WFI or Return from ISR was used for entry:
Any EXTI lines configured in Interrupt mode (the corresponding EXTI
Interrupt vector must be enabled in the NVIC). The interrupt source can
be external interrupts or peripherals with wake-up capability.

 
If WFE was used for entry and SEVONPEND = 0
Any EXTI lines configured in event mode.

 

If WFE was used for entry and SEVONPEND = 1:
– Any EXTI lines configured in Interrupt mode (even if the corresponding
EXTI Interrupt vector is disabled in the NVIC). The interrupt source can
be an external interrupt or a peripheral with wake-up capability. 

 

@QSHAO.1  @TDK   hello I configured PB6 as an external input interrupt. The configuration is as follows, and I am certain that this function is normal and effective.

EXTI_InitTypeDef EXTI_InitStructure;
  NVIC_InitTypeDef NVIC_InitStructure;


  RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);


  SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOB, EXTI_PinSource6);

  EXTI_InitStructure.EXTI_Line = EXTI_Line6;
  EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;
  EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling;
  EXTI_InitStructure.EXTI_LineCmd = ENABLE;
  EXTI_Init(&EXTI_InitStructure);

  NVIC_PriorityGroupConfig(NVIC_PriorityGroup_4);


  NVIC_InitStructure.NVIC_IRQChannel = EXTI9_5_IRQn;
  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x03;
  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x03;
  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
  NVIC_Init(&NVIC_InitStructure);

 And I placed the low-power mode in the time slice polling. Meanwhile, the PB6 pin is self-resetting and will only be triggered once at a time.

 PWR_EnterSTOPMode(PWR_Regulator_LowPower, PWR_STOPEntry_WFI);
    SystemInit();

Show your full code.

If you feel a post has answered your question, please click "Accept as Solution".

Seems your code is normal and effective, then why you ask? 

We ask where you start GPIO CLK, next why you call SystemInit after wake ? ETC.

lan1
Associate II

@MM..1  According to the official data sheet, after exiting the stop mode, the system clock needs to be reset first.

Based on the current transformation, I was certain that entering the stop mode was effective, but when I wanted to exit the low-power mode again, the program did not run normally