2019-08-08 1:00 PM
Is there a HowTo method to program a Nucleo board? I think I inadvertently erased my board and IAR no longer see the ST-Link.
I have tried the following:
Can I recover my Nucleo?
Can I use IAR and the Nucleo's ST-Link?
Solved! Go to Solution.
2019-08-08 2:16 PM
I got it to work.
Informational post only: I had to select ST-LINK/V3 in the Emulator combo box under Project Options, Debugger, ST-Link, Setup tab. Fairly obvious, but it escaped me for some reason. ha
As an aside, in the process of trying things, I upgraded IAR to v8.40. I never thought to check if ST-LINK/V3 was newly added. I do not know whether v8.11 supports the ST-Link/V3. Just saying.
2019-08-08 2:16 PM
I got it to work.
Informational post only: I had to select ST-LINK/V3 in the Emulator combo box under Project Options, Debugger, ST-Link, Setup tab. Fairly obvious, but it escaped me for some reason. ha
As an aside, in the process of trying things, I upgraded IAR to v8.40. I never thought to check if ST-LINK/V3 was newly added. I do not know whether v8.11 supports the ST-Link/V3. Just saying.
2019-08-30 2:07 AM
Thanks for your answer ! :smiling_face_with_smiling_eyes: