cancel
Showing results for 
Search instead for 
Did you mean: 

How conenct SWDIO?

hafiqat_
Associate

Hello. I was recently advised that STM32F103C8T6 and STLINK-V3MINIE should be soldered directly without an adapter.

VCC with 3V3
GND with GND

SWDCLK with CLK

SWDIO with ?

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

> I was recently advised that STM32F103C8T6 and STLINK-V3MINIE should be soldered directly without an adapter.

This is not true. Using CN4 and a cable to a header on the board is the most common and often the best method.

> SWDIO with ?

SWDIO should be connected to pin 3, "TMS".

TDK_0-1742841405770.png

 

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

4 REPLIES 4
TDK
Guru

> I was recently advised that STM32F103C8T6 and STLINK-V3MINIE should be soldered directly without an adapter.

This is not true. Using CN4 and a cable to a header on the board is the most common and often the best method.

> SWDIO with ?

SWDIO should be connected to pin 3, "TMS".

TDK_0-1742841405770.png

 

If you feel a post has answered your question, please click "Accept as Solution".
Peter BENSCH
ST Employee

@hafiqat_ However, you should be aware that you should buy the STM32F103C8T6 from authorised sources, otherwise the risk of getting counterfeits is almost 100%.

Problem: STMicroelectronics and its software cannot support them, which is why problems regularly occur when debugging and working (very often found here in the community). In such a case, you would have to contact the dealer or the manufacturer of the counterfeit.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

> Using CN4 and a cable to a header on the board is the most common and often the best method.

I don't understand what CN4 is. Is it some kind of adapter? If so, what does it look like?



Again, see the User Manual:

AndrewNeil_0-1742936169086.png

It's a 14-pin header which mates with a standard ribbon cable.

AndrewNeil_1-1742936275273.png

AndrewNeil_2-1742936329907.png

AndrewNeil_3-1742936384869.png