cancel
Showing results for 
Search instead for 
Did you mean: 

Hii...Which debugger has better features ST mini or ST link V3 debugger

Gk.1
Associate II
 
5 REPLIES 5
TDK
Guru

By "ST mini" do you mean STLINK-V3MINI? What does "ST link V3 debugger" refer to?

In any case, STLINK-V3MINI is very recent and should serve you well, unless you need to debug at less than 3V in which case you'll need STLINK-V3SET.

If you feel a post has answered your question, please click "Accept as Solution".
Gk.1
Associate II

Yes i was asking abt stlink-v3 mini...and another one is STLINK�?V3 debugger/programmer....which one has better features?​

Gk.1
Associate II

STLINK-V3 SET*​

Uwe Bonnes
Principal III

"debugger hardware" or "debugger software"?

Both for the hardware and software​