2022-04-19 01:44 PM
Please, can I install the ST-LINK, ST-LINK/V2, ST-LINK/V2-1, STLINK-V3 USB driver dpinst_amd64.exe signed for windows 10 on INTEL i5 hardware platform and Windows 11 SO?
Thanks in advance
Angelo Sorbo
2022-04-19 02:15 PM
Not really Microsoft IT team here.
But can't you go into Device Manager, select the device and get it to Upgrade to a more suitable driver you furnish? Should be able to unpack the .ZIP to a real directory, and then point Windows at it in the "I've got a driver" sense.
You can also run the dpinst too, but Device Manager, or running the .INF should also be options.