2023-02-04 04:19 AM
2023-02-04 05:04 AM
Custom board?
Suggests the ST-LINK is not wired in properly or the MCU is not running
Check voltage on VCAP and NRST pins
Check supplies especially VDDA
2023-02-07 02:03 AM
Hello @sk,
It seems the issue you are facing is a connection problem, try checking the connection of the board/ST-Link or use better cables or check the jumpers.
You can also try erasing the flash using STM32Cubeporgrammer, and make sure to activate the gdb server log in the "Debugger" tab of your debug configuration, this may helped you.
Regards,
Chahinez.