cancel
Showing results for 
Search instead for 
Did you mean: 

hi i am using a STM32H745BIT6 chip it is connecting to the st-link but when i try to debug it its not letting me do it it says the following error:

fMoha.1
Associate II

STMicroelectronics ST-LINK GDB server. Version 5.8.0

Copyright (c) 2020, STMicroelectronics. All rights reserved.

Starting server with the following options:

       Persistent Mode           : Disabled

       LogFile Name              : C:\WORK\NEW_PROJECTS_DEV_BOARD\prototype_1\prototype\CM4\Debug\st-link_gdbserver_log.txt

       Logging Level             : 31

       Listen Port Number        : 61234

       Status Refresh Delay      : 15s

       Verbose Mode              : Enabled

       SWD Debug                 : Enabled

Target connection mode: Attach

Reading ROM table for AP 3 @0xe00fffd0

Hardware watchpoint supported by the target

COM frequency = 4000 kHz

ST-LINK Firmware version : V2J37S7

Device ID: 0x450

PC: 0x1

ST-LINK device status: LOCKUP

Enter STM32_AppReset() function

NVIC_DFSR_REG = 0x00000009

NVIC_CFGFSR_REG = 0x00001100

ST-LINK detects target voltage = 2.94 V

Device in lock up state, possibly "read and debug" protected. Use monitor commands to remove the protection

ST-LINK device initialization OK

Waiting for debugger connection...

Waiting for connection on port 61234...

Accepted connection on port 61234...

Debugger connected

ST-LINK device status: HALT_MODE

Enter STM32_AppReset() function

NVIC_DFSR_REG = 0x00000008

NVIC_CFGFSR_REG = 0x00000000

 ------ Switching to STM32CubeProgrammer -----

     -------------------------------------------------------------------

                      STM32CubeProgrammer v2.7.0-RC1                 

     -------------------------------------------------------------------

Log output file:  C:\Users\FMOHAM~1\AppData\Local\Temp\STM32CubeProgrammer_a20644.log

ST-Link Server is running on port : 7184

ST-LINK SN : 30FF6F065647373734141043

ST-LINK FW : V2J37S7

Board      : --

Voltage    : 2.93V

SWD freq   : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID  : 0x450

Revision ID : Rev V

Device name : STM32H7xx

Flash size : 2 MBytes (default)

Device type : MCU

Device CPU : Cortex-M7/M4

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a20644.srec

 File         : ST-LINK_GDB_server_a20644.srec

 Size         : 39552 Bytes

 Address      : 0x08100000

Erasing memory corresponding to segment 0:

Erasing internal memory sector 8

Error: failed to erase memory

Error: failed to erase memory

Encountered Error when opening C:\ST\STM32CubeIDE_1.2.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.6.0.202101291314\tools\bin\STM32_Programmer_CLI.exe

 ------ Switching context -----

Error in STM32CubeProgrammer

Debugger connection lost.

Shutting down...

i did try to erase all the memory but it says its read protected and i checked in the options bites too there is no protection

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
fMoha.1
Associate II

can any one tell me where should i define i am using an internal clock

below, do i need to ENable HSE or LSE or CRS SYNC?0693W00000KbCCTQA3.png