2021-06-27 12:57 AM
2021-06-27 1:29 AM
If the custom board is more-less identical to the Nucleo, programming it will not be much different from it.
Alternatively, you can first try to program the Nucleo board without mbed.
JW
2021-06-28 12:04 AM
Note that all ST driver files are included in mbed-os repo,
so you ca use mbed-os api and rtos, and also all other ST specific features.