cancel
Showing results for 
Search instead for 
Did you mean: 

ST-LINK Connection Error "DEV_CONNECT_ERR" with Nucleo-H755ZI Board

DUBY24
Associate

Dear Team

I hope this message finds you well.

I am currently working with a Nucleo-H755ZI development board (dual-core STM32H755) and encountering a persistent issue when attempting to program or debug the device using STM32CubeIDE and STM32CubeProgrammer.

The following error message appears:

Error: ST-LINK error (DEV_CONNECT_ERR)

Despite multiple attempts and following several troubleshooting steps—including verifying the BOOT0 configuration, updating the ST-LINK firmware, trying "Connect Under Reset", and attempting a full chip erase via STM32CubeProgrammer—the error persists, and I am unable to establish a connection with the device.

Here is a summary of what I have tried:

Verified all physical connections and USB cables.

Updated ST-LINK firmware.

Attempted connection using “Connect Under Reset” while holding down the Reset button.

Ensured I'm targeting the Cortex-M7 core, not the M4.

Attempted a mass erase in STM32CubeProgrammer.

Verified that no low-power or SWD-disabling firmware is loaded.

I would appreciate any guidance or recommendations you can provide to help resolve this issue. If further information or logs are needed, I would be happy to provide them.

Thank you for your support.

Best regards,

1 REPLY 1
TDK
Super User

How can I recover my STM32H7/STM32H7RS board after... - STMicroelectronics Community

If you feel a post has answered your question, please click "Accept as Solution".