cancel
Showing results for 
Search instead for 
Did you mean: 

Help in picking out a Nucleo-board with integrated USB HS PHY

Davit_Imnaishvili
Associate II

Hello, I need a to find a Nucleo board with 2 12-bit ADCs and at least 2.4 MHz sampling frequency. I also need an integrated external phy for HS usb2.0 data transfer. Which STM32 boards are in correspondence with these requirements? Thanks in advance.

5 REPLIES 5

Start by identifying chips which meet your criteria:

https://www.st.com/en/development-tools/st-mcu-finder-pc.html

https://www.st.com/en/development-tools/stm32-finder.html

Then the Product Page for the chip will identify available evaluation boards ...

My issue is that there is no integrated HS PHY option to filter by. Most of the Nucleo boards meet the ADC requirements, the High-speed PHY is more of a problem.

TDK
Guru

Related/duplicate:

Does STM32H723ZG support High-Speed USB data trans... - STMicroelectronics Community

 

Should be straightforward to find a board with one of those chips.

If you feel a post has answered your question, please click "Accept as Solution".

Hi @Davit_Imnaishvili 

I guess they have already answered your question. you can find more about on-chip Hi-speed PHY on F723xx, STM32H7Sxx8 TM32U5Ax ... and more still not referenced in AN4879. You can filter them in Table 4. USB implementation in STM32 devices: D interface

FBL_0-1724333620055.png

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

BarryWhit
Lead II

NUCLEO-U5A5ZJ-Q

 

BarryWhit_0-1724711155064.png

 

BarryWhit_2-1724711252118.png

BarryWhit_1-1724711217479.png

 

- If someone's post helped resolve your issue, please thank them by clicking "Accept as Solution".
- Please post an update with details once you've solved your issue. Your experience may help others.