cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I would like to purchase from you an evaluation board with your STM32F407IET. Do you have any refdesign to share with this MCU? Kind regards Károly

KMusz.1
Associate II

I need to evaluate your MCU of type STM32F407IET

Do you have any evalboard with this device?

Kind regards

Károly

16 REPLIES 16

Dear Khouloud,

Could you send for me the detailed schematics of the following board? Thank you!

[cid:

image001.png@01D70F40.075E1990

]

Kind regards

Hello @KMusz.1​ ,

I cannot see the " [cid:image001.png@01D70F40.075E1990] ".

Could you please give me the board part number so that I can help you?

Thanks, Khouloud

Dear Khouloud,
This board:
[cid:image001.png@01D711D4.1CAD7E30]

Don't attach images via email, we can't see them here. Come to your post/thread, reply and in-line your images, uploading via the Mountain-Sun Icon below left. Or just write the name and part number..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
STM3240G Eval Board
Hello Dear ST,
In your Reference Manual RM0090
On sheet 1132 Chapter 33.4.3. Reduced media-independent interface: RMII
You have this figure:
[cid:image003.jpg@01D7209F.4D40CBE0]
Do you know what is signal CRSDV?
Where is this explained?
Kind regards
Károly Muszka
In your datasheet:
STM32F405xx STM32F407xx
The RMII_CRX_DV and RMII_CRS_DV is mismatched!
Which is correct?
Is this signal mandatory for the RMII 7 pin interface?
Kind regards
Károly