cancel
Showing results for 
Search instead for 
Did you mean: 

H745ZI-Q, NoST-Link detected

MariuszTerebecki
Associate II

I have an H745ZI-Q board. I use it only with default settings. I have connected and programmed it on three different computers for learning purposes. At some point, the board stopped connecting to the computer. In STM32CubeProgrammer, the Serial Number field shows 'No ST-Link detected,' and under Linux, messages appear regardless of whether BOOT0 is connected to VDD or not.

[ 2316.864737] usb usb1-port8: attempt power cycle
[ 2317.276368] usb 1-8: new full-speed USB device number 76 using xhci_hcd
[ 2317.276560] usb 1-8: Device not responding to setup address.
[ 2317.484673] usb 1-8: Device not responding to setup address.
[ 2317.692415] usb 1-8: device not accepting address 76, error -71
[ 2317.820414] usb 1-8: new full-speed USB device number 77 using xhci_hcd
[ 2317.820602] usb 1-8: Device not responding to setup address.
[ 2318.028593] usb 1-8: Device not responding to setup address.
[ 2318.236406] usb 1-8: device not accepting address 77, error -71
[ 2318.236550] usb usb1-port8: unable to enumerate USB device

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
MariuszTerebecki
Associate II

How to diagnose if the board got damaged? How to check if the ST-Link is functional? If it indeed got damaged, I would like to know how to verify it. Could I please ask for assistance?

>How to diagnose if the board got damaged?

Most simple : try another board with same cable/PC - do you have any?

+

Your error msg. > usb 1-8: Device not responding to setup address.< : i get similar with a defective USB stick : no useful response at all.

If you feel a post has answered your question, please click "Accept as Solution".

Well they aren't insulators, they are typically conductive, and some time dissipative..

Boards plugged into anti-static foam tend not to function properly.

Place boards on paper or card board, and wear anti-static straps in handling the boards in high static, low humidity environments where static build up is likely.

ST usually has schematics under the "CAD Resources" tabs of the product pages if you want to trace the circuit and probe voltages.

Generally damage is more likely with metal surfaces, or shorts from metal pens and pencils, or wire, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..