cancel
Showing results for 
Search instead for 
Did you mean: 

Failed to execute MI command: load /[user/]/[Project]/STM32CubeIDE/Appli/Debug/Template_XIP_Appli.elf

avantgov
Associate

Using STM32H7S78-DK board with a STM32CubeIDE project that utilizes an external memory loader, which is included in the project structure. when running debug I am getting a failure with the following console output: 

 

 

Error in final launch sequence:

Failed to execute MI command:
load /[User]/[Project]/STM32CubeIDE/Appli/Debug/Template_XIP_Appli.elf 

Error message from debugger back end:
Load failed ,Failed to execute MI command:
load /[User]/[Project]/STM32CubeIDE/Boot/Debug/Template_XIP_Boot.elf 

Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load /[User]/[Project]/STM32CubeIDE/Appli/Debug/Template_XIP_Appli.elf 

Error message from debugger back end:
Load failed ,Failed to execute MI command:
load /[User]/[Project]/STM32CubeIDE/Boot/Debug/Template_XIP_Boot.elf 

Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load /[User]/[Project]/STM32CubeIDE/Appli/Debug/Template_XIP_Appli.elf 

Error message from debugger back end:
Load failed
Load failed
Failed to execute MI command:
load /[User]/[Project]/STM32CubeIDE/Boot/Debug/Template_XIP_Boot.elf 

Error message from debugger back end:
Error finishing flash operation
Error finishing flash operation

 

 

 Similar forum posts have recommended actions such as running the project with BOOT0 set, clearing out the flash memory with cubeprogrammer, and running the reset behavior as None. None of these have been successful or changed the error message. Console output is below, asking for any help or recommendation on how to resolve this error? Running STMCubeIDE on ubunutu LTS 20.04 

 

 

STMicroelectronics ST-LINK GDB server. Version 7.8.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.

Starting server with the following options:
        Persistent Mode            : Disabled
        Logging Level              : 1
        Listen Port Number         : 61234
        Status Refresh Delay       : 15s
        Verbose Mode               : Disabled
        SWD Debug                  : Enabled
        InitWhile                  : Enabled

Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
      -------------------------------------------------------------------
                        STM32CubeProgrammer v2.17.0                  
      -------------------------------------------------------------------

Warning: The external loader file does not exist:
Template_XIP_ExtMemLoader.stldr
Encountered Error when opening /opt/st/stm32cubeide_1.16.0/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.linux64_2.1.400.202404281720/tools/bin/STM32_Programmer_CLI
Error in STM32CubeProgrammer
Shutting down...
Exit.

 

 



0 REPLIES 0