cancel
Showing results for 
Search instead for 
Did you mean: 

F070F6 Device with Device ID F04x?!

Zt Liu
Senior III
Posted on July 12, 2017 at 09:01

Hi, I am not sure if it's an proper question to ask here, but I ask it here anyway.

I've got some lovely tiny STM32F070F6P6 (with THIS package information on mcu) from china distributor.

Custom boards are made, chips are mounted.

When I start the ST-Link utility, it gives the following message:

0690X00000602U2QAI.bmp

Is this normal?

Or it's just a cloned F070, but with more functions like F04x?!

#stm32-f0 #st-link-utility #device-id
4 REPLIES 4
Zt Liu
Senior III
Posted on July 12, 2017 at 09:28

I should remark that this presumed F070 is currently running a USB CDC function without any problem.

Zt Liu
Senior III
Posted on July 20, 2017 at 04:37

I've just received my new 

STM32F070F6P6 from MOUSER ...

Surprisingly the device ID is still 0x445 which means it's a F04x device.

I try to build some project for F040 and initialize some peripherals which don't exist in F030, (like I2S),

amazingly, it's working!!??

What can I do about this?

.Zt

Posted on July 20, 2017 at 06:09

ST has been know to ship parts with more advanced die than the marking would suggest. If the F04x is a super-set of the F070 then that is a possibility.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
BHama
Associate

0690X000006D4BFQA0.jpgI have problem with STM32 loader as the picture : There is no device number and device ID !