cancel
Showing results for 
Search instead for 
Did you mean: 

External flash loader program not working

I am trying to develop an st-link utility external spi flash loader using STM32F411RE and Winbond W25Q32. Mass erase, Read, Sector erase are working well but the program not working, the following errors are pop-up 

1)Timeout during flash programming.

2)Error occurred during program operation!

3)Programming error @: 0x000010AC.

I also attached my full project file, please review and give suggestions

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Imen.D
ST Employee

Hello @User16438042334827474767​ and welcome to the STM32 Community,

Which version are you using ?

Could you try STM32Cubeprogrammer software. Then, please let me know if this solved your issue.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

1)I used the version attached, please check

2) I also tried the cube programmer v2.4.0 , but I got the same result but new things happened. First mass erases work well and again when I do the same the mass erase fails. My log is given below.

13:34:36 : Disconnected from device.

13:34:37 : ST-LINK SN : 0670FF535155878281143214

13:34:37 : ST-LINK FW : V2J37M26

13:34:37 : Voltage : 3.25V

13:34:37 : SWD freq : 4000 KHz

13:34:37 : Connect mode: Normal

13:34:37 : Reset mode : Software reset

13:34:37 : Device ID : 0x431

13:34:38 : UPLOADING OPTION BYTES DATA ...

13:34:38 : Bank : 0x00

13:34:38 : Address : 0x40023c14

13:34:38 : Size : 8 Bytes

13:34:38 : UPLOADING ...

13:34:38 : Size : 1024 Bytes

13:34:38 : Address : 0x8000000

13:34:38 : Read progress:

13:34:38 : Data read successfully

13:34:38 : Time elapsed during the read operation is: 00:00:00.008

13:34:49 : MASS ERASE ... 

13:34:57 : Mass erase successfully achieved

13:34:57 : UPLOADING ...

13:34:57 : Size : 1024 Bytes

13:34:57 : Address : 0x8000000

13:34:57 : Read progress:

13:34:57 : Data read successfully

13:34:57 : Time elapsed during the read operation is: 00:00:00.007

13:35:10 : MASS ERASE ... 

13:35:15 : Error: Mass erase operation failed.Please verify flash protection

13:35:19 : Memory Programming ...

13:35:19 : Opening and parsing file: images.bin

13:35:19 : File : images.bin

13:35:19 : Size : 101252 Bytes

13:35:19 : Address : 0x00000000 

13:35:19 : Erasing memory corresponding to segment 0:

13:35:20 : Erasing external memory sectors [0 24]

13:35:25 : Error: failed to erase memory

13:35:25 : Error: failed to erase memory

Hi @User16438042334827474767​ ,

I recommend you to update the STM32Cubeprogrammer V2.7.0 and upgrade the ST-Link firmware version (go to ST-LINK>firmware update), then try again and tell me if that solve the issue.

I added the right topics to your question in order to increase its chance to be reviewed by our experts.

Hello @Houda GHABRI​ 

Can you please help @User16438042334827474767​  on this issue.

Thanks

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

thanks for your suggestions but still have the error

 15:16:11 : Disconnected from device.

 15:16:12 : ST-LINK SN : 0670FF535155878281143214

 15:16:12 : ST-LINK FW : V2J37M26

 15:16:12 : Board    : NUCLEO-F091RC

 15:16:12 : Voltage   : 3.24V

 15:16:12 : SWD freq  : 4000 KHz

 15:16:12 : Connect mode: Normal

 15:16:12 : Reset mode : Software reset

 15:16:12 : Device ID  : 0x431

 15:16:12 : Revision ID : Rev A

 15:16:12 : UPLOADING OPTION BYTES DATA ...

 15:16:12 :  Bank     : 0x00

 15:16:12 :  Address    : 0x40023c14

 15:16:12 :  Size     : 8 Bytes

 15:16:12 : UPLOADING ...

 15:16:12 :  Size     : 1024 Bytes

 15:16:12 :  Address    : 0x8000000

 15:16:12 : Read progress:

 15:16:12 : Data read successfully

 15:16:12 : Time elapsed during the read operation is: 00:00:00.007

 15:16:31 : MASS ERASE ... 

 15:16:39 : Mass erase successfully achieved

 15:16:39 : UPLOADING ...

 15:16:39 :  Size     : 1024 Bytes

 15:16:39 :  Address    : 0x8000000

 15:16:39 : Read progress:

 15:16:39 : Data read successfully

 15:16:39 : Time elapsed during the read operation is: 00:00:00.007

 15:16:51 : Memory Programming ...

 15:16:51 : Opening and parsing file: images.bin

 15:16:51 :  File     : images.bin

 15:16:51 :  Size     : 101252 Bytes

 15:16:51 :  Address    : 0x00000000 

 15:16:51 : Download in Progress:

 15:17:56 : Error: failed to download Segment[0]

 15:17:56 : Error: failed to download the File