cancel
Showing results for 
Search instead for 
Did you mean: 

Error: No STM32 target found!

Vimal_M_A
Associate II

Im using Nucleo-H755 i have using this board for the last 3 months usually i get some Errors like no target found but i have solved those by viewing in the community chats but this Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication i have tried every thing i know and suggestions in the other posts like connect under reset , boot0 high , power down mode but i couldnt get it connected while connect the board  there is a file in the H755 storagenamed FAIL.txt in that this msg is present The interface firmware FAILED to reset/halt the target MCU is there any other way to flash the board 

1 ACCEPTED SOLUTION

Accepted Solutions

@Vimal_M_A wrote:

yes im sure i always set smps only 


Sorry I didn't understand. The issue I mentioned previously is indeed when you set the power in SMPS but CubeMX set both SMPS and LDO. Check your project preprocessor.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

14 REPLIES 14
Andrew Neil
Super User

What tool & version are you using to do the flashing - STM32CubeProgrammer?

Are you using the onboard ST-Link?

What does it show for the Target voltage?

https://community.st.com/t5/stm32-mcus-boards-and-hardware/failed-to-execute-mi-command-target-remote-localhost-61234/m-p/764370/highlight/true#M23571

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

17:56:58 : ST-LINK SN : 001A003F3233511739363634
17:56:58 : ST-LINK FW : V3J15M7
17:56:58 : Board : NUCLEO-H755ZI-Q
17:56:58 : Voltage : 3.26V
17:56:58 : Error: Unable to get core ID
17:56:58 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication

Thanks.

What tool & version are you using to do the flashing - STM32CubeProgrammer?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
KnarfB
Super User

Try STM32CubeProgrammer with Reset Mode Under Reset. This might help in cases where a bad firmware disconnectes the SWD debug interface or goes to some low-power modes soon *after* reset.

You may also play with the other settings, like reducing the speed. 

hth

KnarfB

tried that also still not able to connect

 

Vimal_M_A
Associate II

Is there any other way to flash the Microcontroller

please let me know

Use the System Bootloader?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

can you explain how to do that 

 

Hello,

Are you sure you set SMPS instead of LDO for power configuration on this board (Nucleo-H755)? 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.