cancel
Showing results for 
Search instead for 
Did you mean: 

Error: failed to erase memory

SRebe.1
Associate

Hello there

I was trying to debug my stm32h750 with an stlink-v3 mini. I'm currently working with an external flash as my code area. The bootloader and external loader worked before, but suddenly I can't load code on my external flash. Does anyone know why this happens?

This is the error I receive when trying to debug:

STMicroelectronics ST-LINK GDB server. Version 6.0.0
Copyright (c) 2021, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
        Persistent Mode            : Disabled
        Logging Level              : 1
        Listen Port Number         : 61234
        Status Refresh Delay       : 15s
        Verbose Mode               : Disabled
        SWD Debug                  : Enabled
        InitWhile                  : Enabled
 
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
      -------------------------------------------------------------------
                       STM32CubeProgrammer v2.9.0-RC01                  
      -------------------------------------------------------------------
 
ST-LINK SN  : 002F00225632500820313236
ST-LINK FW  : V3J9M3
Board       : STLINK-V3MINI
Voltage     : 3.28V
SWD freq    : 24000 KHz
Connect mode: Under Reset
Reset mode  : Hardware reset
Device ID   : 0x450
Revision ID : Rev Y
Device name : STM32H7xx
Flash size  : 128 KBytes
Device type : MCU
Device CPU  : Cortex-M7
BL Version  : 0xd2
 
 
 
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a30988.srec
  File          : ST-LINK_GDB_server_a30988.srec
  Size          : 312284 Bytes
  Address       : 0x90000000 
 
 
Erasing memory corresponding to segment 0:
Erasing external memory sectors [0 4]
Error: failed to erase memory
 
 
Error: failed to erase memory
Shutting down...

Thanks

1 REPLY 1
Bubbles
ST Employee

Hi @SRebe.1​ ,

is erasing of the external memory working using other means such as the MCU code or a compatible programmer?

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.