2021-06-02 7:47 AM
Hi, I have a discovery board stm32f746 with witch i cannot connect anymore on the st-link port.. Windows does not detect anymore the st-link port .. i took out the chip put it on a smal test board and the chip it's ok is detected as st-link... but on the main board does not, i could connect an external programmer on the 4 pins for programming the st-link... but it still not detected by windows. Please help me recover the board.
2021-06-02 7:53 AM
Isn't the 4-pin to program the on-board ST-LINK?
Which chip did you remove?
Check the USB connector/integrity
2021-06-02 7:56 AM
The st-link chip stm32f103 !
2021-06-02 7:57 AM
i can connect on that chip with external programmer for program it but without the st-link connection i cannot flash the mainboard
2021-06-02 8:02 AM
I put the chip on this board and is detected as st-link chip ... but on mainboard does not... the usb port connector is ok, cable changed, pc changed, no matter what the st-link is not detected is like i'm not connecting the usb cable to the pc... no sound no undected hardware or st-link.
2021-06-02 8:04 AM
I forgot to tell there is a red led that flash all the time when i connect the st-link cable