cancel
Showing results for 
Search instead for 
Did you mean: 

Discovery board stm32f746 with i cannot connect anymore on the st-link port

Argous
Associate II

Hi, I have a discovery board stm32f746 with witch i cannot connect anymore on the st-link port.. Windows does not detect anymore the st-link port .. i took out the chip put it on a smal test board and the chip it's ok is detected as st-link... but on the main board does not, i could connect an external programmer on the 4 pins for programming the st-link... but it still not detected by windows. Please help me recover the board.

5 REPLIES 5

Isn't the 4-pin to program the on-board ST-LINK?

Which chip did you remove?

Check the USB connector/integrity

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Argous
Associate II

The st-link chip stm32f103 !

Argous
Associate II

i can connect on that chip with external programmer for program it but without the st-link connection i cannot flash the mainboard

Argous
Associate II

0693W00000BZuYIQA1.jpgI put the chip on this board and is detected as st-link chip ... but on mainboard does not... the usb port connector is ok, cable changed, pc changed, no matter what the st-link is not detected is like i'm not connecting the usb cable to the pc... no sound no undected hardware or st-link.

Argous
Associate II

I forgot to tell there is a red led that flash all the time when i connect the st-link cable