cancel
Showing results for 
Search instead for 
Did you mean: 

Digital inputs in STM32 boards ?

AElta.1
Associate II

I am working on reading an External 3 bit parallel CMOS ADC (4-8 MSPS)(from MAX2771 board or Eva KIT) GNSS digital output. I want to read this digital output pins using the NUCLEO-H723ZG, I do not know if there is digital inputs pin in the board ?

if so what is speed of the GPIO pins ?

thanks in advanced

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

All the pins in the GPIO bank (16 pins) can be read via GPIOx->IDR. Could perhaps use a TIM input pin to trigger DMA.

​

F​or a clocked parallel input, perhaps look at DCMI

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Super User

@AElta.1​ "using the NUCLEO-H723ZG, I do not know if there is digital inputs pin in the board ?"

The User Manual has details of all available pins - inputs, outputs, etc.

Also look at the schematics.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.