2020-07-03 3:33 AM
I am working with Windows10, STM32CubeIDE V.1.3.1 and ST-Link on board of NUCLEO-L412KB. Today i connected the board first time and made an update after being asked to do so. After reconnecting the board and successfully update of ST-Link the debugger lost it's connection after starting debugging process.
STMicroelectronics ST-LINK GDB server. Version 5.5.0
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Debugger connection lost.
Shutting down...
After that, the Debugger LED on NUCLEO board remains red until i restart my PC. After restart, the LED lights up green, but after starting debugging process all is the same behavior like before.
Please help!
2020-07-09 5:22 PM
Something similar did happen to me .
I do pinpoint ,after it does the St-link upgrade cause that problem, in the future I will not do the upgrade until STM fix bugs.
Anyway the way how I did overcome this problem; after following instructions from another St community member.
Delete all projects currently on your workbench, and start a fresh project from scratch .
And its working on Windows 7,8 and 10
Hopefully fix and good luck
Jorge