cancel
Showing results for 
Search instead for 
Did you mean: 

Code generation issue with Discovery board B-L072Z-LRWAN1

NicRoberts
Senior II

I have a Discovery board B-L072Z-LRWAN1 and I am trying to set up a project using CubeIDE but get the following,

NicRoberts_0-1768308697317.png

So I check to see if the L0 & LRWAN packages are in the repository,

NicRoberts_1-1768308848946.png

Yes, they're there. I click OK & Cube carries on setting itself up & up pops the ioc window. I press configure & generate & get some C code but the build option is greyed out.

 

What am I missing here?

 

 

 

10 REPLIES 10

Thanks Mattias, I was confused about why it wasn't finding the FW in the repository as this wasn't an issue with any of the other boards we use.