2020-12-06 4:22 AM
Hi,
I just powered up my own board and i just wanted to start debuging.
The first thing i tried was to connect with the STM32 ST-Link Utility and an ST-Link V2.
This works fine. I can connect via SWD and can read the Chip-ID and see the Flash.
In terms of the hardware everything seemed to be fine for me.
So i continued with setting up the newest Cube IDE which i just downloaded. (Version: 1.5.0)
I set up an example project, with my processor and SWD enabled and tried to start debugging. But this is where i encountered the problem. When i was starting the debugging session, it took forever to connect, showing the following debug log:
STMicroelectronics ST-LINK GDB server. Version 5.7.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.6.0-RC3
-------------------------------------------------------------------
ST-LINK SN : 52FF6D067189554829302567
ST-LINK FW : V2J37S7
Board : --
Voltage : 2.48V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x422
Revision ID : Rev Y
Device name : STM32F302xB-xC/STM32F303xB-xC/F358xx
Flash size : 128 KBytes
Device type : MCU
Device CPU : Cortex-M4
this took some minutes.
and the following progress status appeared for some time:
After some time, the debugging session showed the following log:
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a05992.srec
File : ST-LINK_GDB_server_a05992.srec
Size : 6340 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 3]
Error: failed to erase memory
Error: failed to erase memory
Encountered Error when opening C:\ST\STM32CubeIDE_1.5.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.5.0.202011040924\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
How can i resolve this issue?
I am open for any suggestions.
Best Regards
Markus
Solved! Go to Solution.
2020-12-06 5:34 AM
Resolved! - the problem was caused by an instable power supply!
2020-12-06 4:31 AM
Just a small addition to my problem - i am using Windows 10 - just for you to know if this can be related to such a Problem
2020-12-06 4:36 AM
Just found out, that a full chip erase in stm32 st-link utility wont complete and does not work.
2020-12-06 5:34 AM
Resolved! - the problem was caused by an instable power supply!