cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot connect to STM32G0B1 custom board

degaus
Associate II

Hello everyone,

I have designed a custom board with the STM32G0B1CET6N but I cannot connect to the nucleo st-link programmer.

I have removed the two jumpers from the nucleo board but when connecting to the board it doesn't get recognised by the ST-Link Utility or STM32Programmer.

degaus_0-1731863186909.png

degaus_1-1731863209776.png

I do get an issue with the driver on the Device Manager but when I connect it to another custom board it works fine.

degaus_2-1731863258999.png

Below is the schematic for my custom board.

degaus_3-1731863332157.png

Any help is really appreciated.

 

Matteo

 

11 REPLIES 11
degaus
Associate II

Hi MM..1,

 

Thanks again for your help.

 

I have connected as your suggestion and now I do get a different error.

degaus_0-1731879470669.png

degaus_1-1731879498625.png

Need more investigation...I may get the board re-done with the VDDIO2 and VSS connected this time, just to make sure that the flying wires are not connected properly.

PS. Could you please let me know if I missed something else from schematic?

Thanks again.

Matteo

 

Pavel A.
Evangelist III

I am new on STM32 so forgive me for silly mistakes.

Desire of using ST-link of other ST board instead of a normal modern ST-link v3 (high speed, VCP) is one of these mistakes IMHO. Just doubles chance of damage and confusion, for nothing good.