cancel
Showing results for 
Search instead for 
Did you mean: 

Can't set 8 bit diplay type on LTDC Controller for STM32H723ZGTX

LPZ
Associate

Good morning,

for a project I have to set the LTDC display type to be 8 bit for some bottleneck, but doing that on STMCubeMX for my MCU STM32H723ZGTX there are only 24, 18 and 16 bit configs available.
How can I set this value to be 8 bit?
Thanks for the patience

4 REPLIES 4
MNapi
Senior III

what kind of display you are talking about ?  there are a few of them to use 8 bit data.

 

1.png

@MNapi here, he's talking about a display through LTDC interface and not via FMC.

@LPZ I'm not an expert of that peripheral but from the AN4861 table 4:

SofLit_0-1718388423518.png

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

if he is talking LTDC then we would have something like RGB323 format.

You would use pins R7, R6, R5, G7, G6, B7, B6, B5. Nobody is using something like this.

There is no such a thing.

RGB565 is the most popular.

a have a few projects connected to 8 bit TFT and you use FMC not LTDC

I agree. But it depends on his HW constraints: availability of FMC pins? power consumption etc ..

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.