2020-10-18 04:01 AM
There is no fully communication with ST-link V2 with STM32 Link utility program.
All drivers installed properly, signed.
Firmware upgrade mode works, programming mode not.
FW version: V2J33s7
I set low rate speed 100 kHz, try all reset options - never work.
STM target information - detection fail
What I can do now?
2020-10-18 05:16 AM
Make sure pin 1 or 2 is connected to board supply, and target voltage is reporting correctly.
Would need more info on target boards and attachment to understand why.