cancel
Showing results for 
Search instead for 
Did you mean: 

Can i set a LED output register on DISCOVERY board with SWD.

Patrick Morwald
Associate II
Posted on July 11, 2017 at 16:09

Hi,

i wondered if i can use the &sharpSWD in &sharpST-Link on the STM32F407G-DISCO1 Board to set individual IO registers during runtime?

According to

https://www.arm.com/products/processors/serial-wire-debug.php

it can be used as AMBA bus master to manipulate IO registers...

So consider the simple test case: I want to switch on the red onboard LED (PD14) on the DISCOVERY board with SWD during runtime. How do i do it? What client software would you recommend? 

I tried SW4STM32 but couldnt write the IO registers during runtime, no idea why it did not work.

I also used ST-LINK CLI and read memory address 0x40020C00 - 0x40020FFF (GPIO D memory area) but i only got zeros....

Am i using the SWD in the wrong way? Please help!

Patrick

#swd #stm32f4 #st-link
This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Posted on July 11, 2017 at 16:54

>>

I also used ST-LINK CLI and read memory address 0x40020C00 - 0x40020FFF (GPIO D memory area) but i only got zeros....

Did you enable the clock first?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Patrick Morwald
Associate II
Posted on July 11, 2017 at 17:00

Hi,

i wanted to update: I can manipulate the IO registers now through sw4stm32 with the plugin 'EmbSys Registers'. 

However, how do i do it with ST-LINK CLI? Is it even possible to read out peripheral register addresses with this tool? 

Please clarify!

Patrick

Posted on July 11, 2017 at 17:01

The peripheral clock is activated. I am running an application on the device where it gets activated right on startup.

Patrick Morwald
Associate II
Posted on July 12, 2017 at 10:12

Hi,

update again: I can manipulate the IO register successfully with ST-LINK GUI. That means i can toggle an LED via register write now, but still i get a write error message popup in the GUI.

However, it doesnt work in the command line tool. I always get a write error:

C:\Users\pm>ST-LINK_CLI -w32 0x40020C18 0x00004000

STM32 ST-LINK CLI v3.0.0.0

STM32 ST-LINK Command Line Interface

ST-LINK SN : 066EFF575450707267193852

ST-LINK Firmware version : V2J28M18

Connected via SWD.

SWD Frequency = 4000K.

Target voltage = 2.9 V.

Connection mode : Normal.

Device ID:0x413

Device flash Size : 1024 Kbytes

Device family :STM32F405xx/F407xx/F415xx/F417xx

Writing 0x00004000 at 0x40020C18... Error!

Can anyone say what i am doing wrong in the command line tool? Please help!

Patrick

Posted on July 12, 2017 at 17:51

>>

Can anyone say what i am doing wrong in the command line tool? Please help!

Looks like a limitation in the software, this is a user forum, help depends on others working in a similar area. If you are a commercial client, push in via the sales and FAE contacts.

I've flagged this post for attention.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Imen.D
ST Employee
Posted on July 13, 2017 at 13:38

Hello,

I raised this issue internally to the ST-Link responsible and it's under investigation.

I will come back to you as soon as I have needed details.

With Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen