2017-07-10 6:59 AM
Hi
I bought a new NUCLEO F207ZG, i plugged it to my computer but it detects nothing, there is no unknown device in the device manager window. The COM led is just blinking, and the initial program is running making the User Leds blinking by pressing the User button.
How can i fix this?
I am running on Windows 10.
This board uses a USB micro B to plug to PC while all works fine with an F429I Discovery which uses a USB mini-B.
#stlink2017-07-10 10:17 AM
>>
there is no unknown device in the device manager window
Survey says : Drivers
The F429-DISCO isn't mbed compatible as I recall, the NUCLEO-144 is, needs a newer set of drivers supporting the ST-LINK V2-1
2017-07-11 3:44 AM
I fixed it. I was just using faulty usb A/micro usb B cables. I bought a new cable and it works.