2020-10-19 10:10 PM
I want to quickly verify the SWD debug interface of my new H7 MCU. These is no firmware can be downloaded to MCU so that I need to just verify the MCU and debug can work. It is pure hardware test.
Solved! Go to Solution.
2020-10-20 06:25 AM
Open STM32CubeProgrammer and try to connect to the chip.
2020-10-20 06:25 AM
Open STM32CubeProgrammer and try to connect to the chip.
2020-10-20 09:37 AM
I just installed STM32CubeProgrammer tool on my PC. I can not open it after a very short start screen.
2020-10-20 09:53 AM