cancel
Showing results for 
Search instead for 
Did you mean: 

Can I quickly verify SWD debug interface with ST-LINK/V2?

JZou.2
Associate II

I want to quickly verify the SWD debug interface of my new H7 MCU. These is no firmware can be downloaded to MCU so that I need to just verify the MCU and debug can work. It is pure hardware test.

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

Open STM32CubeProgrammer and try to connect to the chip.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
TDK
Guru

Open STM32CubeProgrammer and try to connect to the chip.

If you feel a post has answered your question, please click "Accept as Solution".
JZou.2
Associate II

I just installed STM32CubeProgrammer tool on my PC. I can not open it after a very short start screen.

Let's pretend I can't see what's happening on your computer.
Why can't you open it? What happens? Do you see error messages? Did you follow the instructions of those messages?
If you feel a post has answered your question, please click "Accept as Solution".