2021-09-28 4:54 AM
I've attached the schematic of the MCU. In my application, I'll be using sensors, LoRa, and a PWM output. I have prepared the schematic considering the situation that I'll be able to upload a program to the MCU on board. Please let me know if anything is wrong with this. Your prompt response is going to help me a lot.
Thank you.
2021-09-28 8:11 AM
What is the best way to solve it, can you please tell me? So that I can upload the program once and it will run throughout time.
2021-09-28 9:52 AM
If I use an ST-LINK V2, whose pins are as shown as follows.
will it work if I connect the following?
Aksing you to get confirmation. In this way can I debug and upload the program to MCU instead of a complicated BOOTloader and UART? If so, should I pulldown BOOT0 to the ground?
2021-09-28 9:43 PM
If I do this, will it add debug functionality and work well? I have connected BOOT0 to GND this time and STLINKV2, 2 pins to MCU's required 2 pins. As per the datasheet, these 2 pins can be sufficient to debug. What is your opinion on this?