2023-05-15 6:42 AM - last edited on 2025-11-28 8:13 AM by Andrew Neil
STM32F103CBT6 is the same MPU used on the Nucleo demo boards as an ST-Link implementation.
Is it possible to get these processors pre-programmed with ST-Link firmware?
Under what conditions, if any?
2023-05-15 7:09 AM
Welcome, @MUmmi.1, to the community!
unfortunately, the ST-Link firmware is proprietary and therefore cannot be distributed, either as a binary or pre-programmed on an STM32. The only legal way to get it is by buying an ST-LINK/V2 or ST-LINK/V2-1 (part of many NUCLEO and some DISCOVERY boards).
Does it answer your question?
Regards
/Peter
2023-05-15 7:13 AM
Hi Peter,
Thanks for your prompt response. Is ST-LINK/V2 been supported or is it ST-LINK /V3 ?
2023-05-15 7:34 AM
What do you mean by "is been supported..."?
STM32F103 is only included on the ST-LINK/V2 or /V2-1, the ST-LINK/V3 contain a different STM32.
2023-05-15 7:37 AM
Hi Peter,
My apologies , was a typo . I meant to ask if STM32F103 supports ST-LINK/V3 as well.
Based on your response, I have gotten the answer.
Thanks
2023-05-15 7:45 AM
OK, you're welcome!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter
2023-05-15 9:07 AM
The ST-LINK/V3 uses a STM32F723 part, so no the STM32F103 does not support the same feature set as it is a smaller and more restricted device.
We should be pushing ST toward supporting CMSIS-DAP in their tools
2023-05-15 12:12 PM
That's really helpful, Thanks DeLorean