cancel
Showing results for 
Search instead for 
Did you mean: 

Any new Nucleo boards this year?

kj.obara
Associate III

Hi everyone, I just wondered if anyone is privy to information if STMicroelectronics is still in the maker business, that is do they plan any new Nucleo boards for hobbyists this year? Or maybe that was too much hassle for the company and not worth it apart from the initial kick start?

I'm dreaming of a new board with Nucleo-32 format but with a 48-pin chip so that none of the 30 board pins are NC or if it had a few pins more. If anyone is aware of STM32L4/L4+ chips on boards of the nano format produced by some other manufacturer that would be a great help too.

The reason I'm asking is because I might have to buy a dozen of boards like Nucleo-L432KC, since they are closest to what my ideal board would be, but I wondered if it makes sense to wait a little longer if anything was in the pipeline...

Thank you.

3 REPLIES 3
Amel NASRI
ST Employee

Hi @kj.obara​ ,

Just as an example: NUCLEO-L4P5ZG was delivered with the announcement of NEW STM32L4P5xx/L4Q5xx devices on March this year (see details).

So ST continuous to make such boards :)

The exhaustive list of boards from ST or third parties can be found on https://www.st.com/en/evaluation-tools/stm32-mcu-mpu-eval-tools.html.

I recommend you to use the "Product Selector" to fine tune the selection and apply filters depending on your needs.

If you still "dream" of a board that is not there, I suggest you to submit it in "Idea Zone" (use the category "STM32 MCUs generic").

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Find a generic breakout board

See also boards on eBay, AliExpress, Tindie, etc

Pretty sure Ive seen feather and nano type boards in my travels.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..