cancel
Showing results for 
Search instead for 
Did you mean: 

According to AN4488 for STM32F4 (64-pin in my case), the VDDA pin "must" be connected to two decoupling capacitors. Is this needed for digital-only applications? If not, should the pins be left floating? The ADC seems isolated from the rest of the supply.

xzapu.1
Associate
 
2 REPLIES 2
AScha.3
Chief II

2 caps is "old style" nonsense. ONE 10uF cer. cap is better in any way. just that time, 20 y ago, such cap was non existent . thats why they tried to do put some 10nF , 100nF and 10 uF elko together, generating a nice group of resonances between thees caps. try it yourself, simulate, or just believe it.

one cap, 10uF cer. X7R , and connect to VDD. thats it.

If you feel a post has answered your question, please click "Accept as Solution".

The STM32 have the PLL and RESET circuitry run off the analogue supplies, you really can't leave them unconnected because you're not using the ADC/DAC

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..