2020-05-07 07:42 AM
ST please document the changes.
They used to be documented, sort-of, directly in the schematics (which used to be in the UM); they are not anymore.
And ST, please put back the schematics into the UM. I know you've said it's removed for your convenience, but please put users' comfort in front of yours.
JW
2020-05-12 04:44 AM
Hello Jan,
The changes are as follows:
- New version migrated to Altium and board templates upgrades
- QSPI Micron N25Q128A13EF840F changed in MT25QL128ABA1EW9-0SIT
- LCD Rocktech RK043FN48H-CT672B changed in KUNJIAN HT043C
- MEMS ST MP34DT01TR-M changed in ST IMP34DT05TR
- Oscillator NDK NZ2520SB 25MHz END4869B changed in NDK NZ2520SH 25MHz END4869C
- Oscillator NDK NZ2520SB 24MHz END4869A changed in NDK NZ2520SH 24MHz END4869D
- USB protection ST USBULC6-2F3 changed in ON Semiconductor ESD7383NCTBG
- Memory SDRAM Micron MT48LC4M32B2B5-6A changed in ISSI IS42S32400F-6BL
Regards,
2020-05-12 05:11 AM
Hi @Imen GH
Thanks for the information.
Looking forward to the new UM which undoubtedly will contain all this information! :-)
Jan
2020-05-12 05:13 AM
... and this one is strange...
USB protection ST USBULC6-2F3 changed in ON Semiconductor ESD7383NCTBG
JW