cancel
Showing results for 
Search instead for 
Did you mean: 

ST-LINK/V2 works on CooCox?

edsonrodrigueseca
Associate
Posted on October 29, 2014 at 01:37

Hello.

I am new in ARM development and I am trying CooCox. I want to buy a debugger and I would to know if I will be able to use ST-LINK/V2 with CooCox.

Thanks in advance.

#debug-stm32-using-st-link/v2
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
frankmeyer9
Associate II
Posted on October 29, 2014 at 09:01

Since AFAIK, the integrated ST-Link on the discovery boards is basically a scaled-down version of the standalone debug pod, I would expect Coocox to support it, at least SWD mode.

But I would ask that question on the Coocox forum, too.

edsonrodrigueseca
Associate
Posted on October 29, 2014 at 23:50

Thanks for your reply. I will not use a discovery board.

frankmeyer9
Associate II
Posted on October 30, 2014 at 09:18

I will not use a discovery board.

 

That's what I understood.

ST sells a separate debug pod as ''ST-Link''. The integrated version in the discovery board is obviously derived from that one, both are using the same firmware.

But since Coocox supports several discovery boards, I expect it to support the standalone ST-Link too, at least in SWD mode.

Nickname306_O
Senior
Posted on October 31, 2014 at 17:47

Hi rodrigues.edson,

CooCox toolchain supports ST-Link/V2 Debug Probe.

Best Regards,

Nouha