2016-09-16 04:44 AM
Hello,
I'm trying to communicate with a Mifare classic card but I can't.I'm following the example described on the datasheet (page 60) and when it comes to auth, I'm sending the command:0x04 0x09 0x60 0x00 0x04 0x00 0xd1 0x00 0x3d 0x00 0x18But the answer is alway the same: 0x87 0x00I've tried modifying the frame waiting values, but the error persists.Any idea?Thanks in advance! #cr95hf-st95hfSolved! Go to Solution.
2016-09-26 03:04 AM
Hello ELasa,
As mention in the datatsheet :
MIFARE and MIFARE
®
Classic are trademark of NXP B.V. and are used under license.CR95HF is able to manage the Parity Framing mode compatible with MIFARE
®
classic requirements. However, access to Authenticated state must be support by an external secure host which embeds the MIFARE®
Classic library. So you have to check with the TAG provider specifications in order to manage the entire sequence and protocol which is not natively done by the CR95HF. Regards2016-09-26 03:04 AM
Hello ELasa,
As mention in the datatsheet :
MIFARE and MIFARE
®
Classic are trademark of NXP B.V. and are used under license.CR95HF is able to manage the Parity Framing mode compatible with MIFARE
®
classic requirements. However, access to Authenticated state must be support by an external secure host which embeds the MIFARE®
Classic library. So you have to check with the TAG provider specifications in order to manage the entire sequence and protocol which is not natively done by the CR95HF. Regards