2024-11-22 01:24 AM
Hi,
I am using the st25r3916b to read cards (ISO14443A) and as card emulator. I am not sure if I am using the maximum antenna power. If you could give the clue of which registers and which values should I use to have it with the maximum output power.
Thanks,
Sandra
2024-11-22 05:40 AM
Hi Sandra,
maximum output power is mainly a function of:
Best Regards, Ulysses