2023-05-23 02:35 AM
ST25R3911B-DISCO is not suitable for its GUI. Use the HAL library to write programs to read ST25. Is there a related program?
Solved! Go to Solution.
2023-05-23 04:46 AM
Hi Gfang.2,
I interpret that you want to use a firmware without GUI?
X-CUBE-NFC5 and ST25 Embedded NFC lib for ST25R3911B are examples running on STM32 and using its HAL. Is that what you need?
BR, Ulysses
2023-06-06 05:23 AM
Please check the above mentioned examples out.
2023-05-23 04:46 AM
Hi Gfang.2,
I interpret that you want to use a firmware without GUI?
X-CUBE-NFC5 and ST25 Embedded NFC lib for ST25R3911B are examples running on STM32 and using its HAL. Is that what you need?
BR, Ulysses
2023-05-23 06:20 AM
Yes, need an ST25R application example. Can you provide assistance?
2023-06-06 05:23 AM
Please check the above mentioned examples out.