cancel
Showing results for 
Search instead for 
Did you mean: 

Purpose of A/D register in ST25?

sanjogsapkota
Associate

what is A/D register for? when i bring the st25r tag(sticker one) near the st25 nfc its value changes. And how is interrupt generated? what are the values of registers to be set in order to read a NfC tag?pseudo code for it.

 

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 ACCEPTED SOLUTION

Accepted Solutions

Hi sanjogsakota,

please check the DS, there are a number of direct commands which trigger an A/D conversion and put the result into the mentioned register.

BR, Ulysses

 

View solution in original post

3 REPLIES 3
Brian TIDAL
ST Employee

Hi Sanjog,

which product do you refer to? ST25R3916?ST25R3916B?ST25R3911?

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

i am using ST25R3911B -DISCO but using an external stm32(blue pill)

Hi sanjogsakota,

please check the DS, there are a number of direct commands which trigger an A/D conversion and put the result into the mentioned register.

BR, Ulysses